2935253854

  • Total activity 6
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 2

Activity overview

Latest activity by 2935253854
  • 2935253854 created a post,

    crop the .bag file

    I used the D415 camera to record a bag file, but I only need the video recording after 5s of the file, is there a way to crop the file

  • 2935253854 commented,

    Thank you for your patience

  • 2935253854 commented,

    Whether all realsense camera is fixed or not, the depth map will fluctuate, as shown in the figure below, the area framed with the red rectangle will fluctuate

  • 2935253854 created a post,

    D415 gets the real distance

    When the D415 camera acquires the real distance, does it need to perform operations such as camera calibration, color map and depth map alignment, or can it directly use the get_distance(x,y) funct...