Cuau Lenaic
- Total activity 19
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 2
- Subscriptions 3
Comments
Recent activity by Cuau Lenaic-
Hello everyone, I have exactly the same problem as you. I would like to improve the accuracy of my D405 camera in presence of untextured surfaces. First MartyG what would give the best surface qua...
-
Oh yes the idea seems good. However, my laser works in range 10-30 mm only and now it is already at the maximum range.
-
Here is an example of what I mean when I talk about "laser disturbance", I observed it some days ago (2 images down). However, today, for a reason I cannot explain in the realsense viewer the surfa...
-
It is baby powder indeed. I used it for reflection and also for making clear white spots to help stereovision triangulation.
-
For position 3 it is not possible because if I do this the laser could not make its measure which is important for me. Yes for now I am doing hole filling , but as the spot is a bit big I miss a lo...
-
You mean between the spot and the camera (position 2 in the following scheme) ? My filter is a little circle of diameter 1.2 cm. So I think in that case it will be hard to hide the laser from left ...
-
The camera is already tilted when I took the image of the spot. And even with another orientation it is not very different. The main problem for me is that is the area of the spot I cannot determin...
-
It looks like my previous comment was not sent (not sure but I try again : )Haha yes I guess it is ressembling to USS Voyager ! But is is just a dome in colored silicone with white powder for stere...
-
I made the settings exactly as you said. The image seems a little bit darker but laser is still a big red spot
-
Unfortunately my laser operates at 660 nm and the camera does see it, which disturbs me for my application, that is why I was looking for a notch filter. But even if the notch filter works very we...