Dafni Xanthopoulou

  • Total activity 8
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 1
  • Subscriptions 1

Activity overview

Latest activity by Dafni Xanthopoulou
  • Dafni Xanthopoulou commented,

    MartyG hi, I realised that there's a lot of macOS Ventura and Monterey problems with the error I'm getting "failed to set power state" or "failed to claim usb interface" and I see some unreliable s...

  • Dafni Xanthopoulou commented,

    @MartyG Thank you. I have tried a few different approaches, but still struggling. My goal now would be to use the infrared image of the realsense (you see I need to use it in a dark environment wit...

  • Dafni Xanthopoulou commented,

    MartyX Grover after building from source the latest SDK editing out the line of code that changes the name from D455 to D456 as suggested, Touch Designer detects the camera as D455 -which is great ...

  • Dafni Xanthopoulou commented,

    Thank you for this insight, I will try to build from source changing the line in the code and let you know how it went.  What I really need to do is skeletal tracking, so If that doesn't work I was...

  • Dafni Xanthopoulou commented,

    Thank you so much or your answer MartyX Grover. I want to find the position and rotation of a camera or an object that the camera is observing. When I say Max/Msp I mean specifically Max 8 by Cycli...

  • Dafni Xanthopoulou created a post,

    RealSense D456 & TouchDesigner

    Hi, I want to use the D456 in TouchDesigner to do Pose Tracking.I have a brand new RealSense D456 connected to a MiniMac (Intel) with MacOS Mojave 10.14, with the librealsense installed and the Rea...