1095425988
- Total activity 10
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Comments
Recent activity by 1095425988-
Hi So, the reason for this problem is that the stem of the plant is too smooth, too little texture, and the structured light camera has difficulty obtaining depth information? Can the sdk enhance t...
-
Thanks, I see, so are the depth maps and rgb maps in the bag files I recorded with the sdk also this kind of subsequently processed or are they raw? And,how should sdk be modified to get the raw de...
-
Yes, my parameters are all taken from the viewer exported csv file and I did notice the difference in the camera.At the moment, I'm wondering if there's something wrong with the way I'm saving the ...
-
yes
-
I followed the instructions in the link to disable GLSL, but the problem persists. And the code I'm using is the open3d teaching case, the camera matrix uses a csv file on save. color_raw = o3d.io....
-
Okay, here's the rgb map with depth map that I saved via realsense.viewer.