Matt

  • Total activity 4
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Matt
  • Matt commented,

    Hi MartyG, thanks for the response. Can you clarify to what point on the camera the 60 cm and 85 cm distances are referring to? Since the tolerance on that distance is fairly tight (+/- 1mm) it mat...

  • Matt commented,

    Copy that. On a similar note, how do I interpret the red and yellow stars in this image? - Is the yellow star the center of the "crease" of the OEM calibration target? Without the CAD model, I'll ...

  • Matt created a post,

    CAD model for the OEM Calibration Target

    Hi! I am designing a physical fixture to hold the D415e and the Intel OEM Calibration target so that I can do the OEM calibration procedure. There are some rough overall dimensions listed on the ca...