H0985630316
- Total activity 13
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Comments
Recent activity by H0985630316-
Are there any recommendations for other methods that I can try? like using an older version or using another OS is more stable for this camera.
-
and sometimes it can detect the camera but cannot work realsense-viewer then the following information appear: 18/12 14:10:58,805 WARNING [281472678097088] (messenger-libusb.cpp:42) control_transfe...
-
Hello, it works successfully but will turn itself off after about 10 minutes, and then turn it on again, and the following information will appear: 18/12 13:28:25,809 WARNING [281473248260288] (sen...
-
hello, I install and then the raspberry can detect the camera device, then I try the command realsense-viewer. It appears the depth camera at very first then given the error bellow. 15/12 15:05:54,...
-
Yes, I tried the link:https://github.com/IntelRealSense/librealsense/blob/master/doc/libuvc_installation.md, and the same error occurs.
-
I also tried the link https://github.com/IntelRealSense/librealsense/issues/11506#issuecomment-1599168850, and the same error occurs.
-
Hello, I remove the command -DBUILD_WITH_CUDA:bool=true, and it still appears error CMake Error at /usr/share/cmake-3.22/Modules/CMakeDetermineCUDACompiler.cmake:179 (message): Failed to find nvcc...
-
Hello, yes. still have this problem
-
Hello, thanks for your help, but when I use the command "make -j 4" the error appears as follows. How can I fix it? /home/pi/projects/librealsense/build/third-party/libcurl/lib/vtls/openssl.c: In ...