Sundaramoorthi S
- Total activity 5
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by Sundaramoorthi S-
Sundaramoorthi S commented,
Hi MartyG, When using a single Intel RealSense D410 with a Raspberry Pi, we've observed that the ASIC temperature of Intel realsense D410 is maintained at 50 degrees Celsius. We are concerned abou...
-
Sundaramoorthi S created a post,
Frame Drop issue
Hi, in our current setup, we have two Intel RealSense D410 cameras connected to a Raspberry Pi 4B. One camera is directly connected via a 0.25m USB 2.0 cable in a USB 3.0 port, while the other uses...
-
Sundaramoorthi S created a post,
Frame Drop issue
hi, I am using Intel Realsense D410 with Raspberry Pi 4B(using realsense viewer 2.50). My resolution is 480 X 270 & FPS - 30 while connecting one sensor, i can able to get 30 FPS , with both Depth ...