Kvuong

  • Total activity 29
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 4

Posts

Recent activity by Kvuong Recent activity Votes
  • Setting D405 Camera Exposure in Python

    Hello, is there a method to set the camera exposure for the Realsense D405 camera? Say, I have an image, then I put a piece of paper to fill up a lot of the screen. The camera will compensate for t...

  • RealSense D405 Depth Map Fidelity

    Hi there, I am using the D405 depth camera to track a marker that I detect using OpenCV. I have a green marker that I track by masking a camera image, then I use the tracked position to retrieve 3D...

  • Retrieving World Coordinates from Image Frame Intel Realsense D415

    Hi, I was wondering if there is a built in function in the RealSense library that can retrieve the millimeter values from an image taken with the D415. I know that we can retrieve depth from the ca...

  • RealSense D415 and D405 Precision

    Hi, I am currently using the Intel RealSense 415 camera to track motion at a close distance (in this case the closest being ~30 to ~40 cm. I am using Python to access the camera's depth frame to re...