Aswaths
- Total activity 5
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Comments
Recent activity by Aswaths-
Thanks for the calculation MartyG. Will discuss with our team and get back to you regarding purchases if it is suitable.
-
Our object is a circle with 1cm diameter placed at a distance of 70cm 10 120cm. The product description of D405 says it has submillimeter accuracy of 0.1mm at 7cm. Do you have any graph which compa...
-
Hi MartyG. Our working distance range is between 70cm to 120cm, So D435 model seems to be good for us. If the error percentage is 1% at this range (120cm) it comes around 1cm, which is far greater ...