Viseshsonigra

  • Total activity 7
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Viseshsonigra
  • Viseshsonigra commented,

    It is not a single board computer. It is actually a gaming PC with fairly decent specs. Attached is the spec sheet for the same.

  • Viseshsonigra commented,

    Hi,  We have bought the recommended cable as per above and are still seeing the camera temperature reaching around 34 degrees. Additionally, we are still getting the USB SCP overflow error and now ...

  • Viseshsonigra commented,

    While we await the new cable, is there any other solution we could employ to mitigate the overheating?

  • Viseshsonigra commented,

    We have purchased a new cable and will do some testing and get back to you.    Thank you once again

  • Viseshsonigra commented,

    The cable is 3m long currently. Unfortunately it would be quite difficult to test with a lower resolution as our use case needs a fairly high resolution to work (I will need to confirm this with th...

  • Viseshsonigra created a post,

    SCP overflow and overheating

    While using the camera, we sometimes get the SCP oerflow error and the temperature shows at 35C; the camera is at a distance from the PC hence are using an extension cable which is 3.0. If we just ...