Victor

  • Total activity 19
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 3

Posts

Recent activity by Victor Recent activity Votes
  • The overexposure issue with realsense d455

    Hi there, I'm using Realsense SDK 2.50.0 along with Realsense ROSv2.3.2. I cannot get good-quality outdoor depth and RGB frames when auto-exposure is on. To avoid sun glare, the camera looks down a...

  • Realsense_ROS Point Clouds Callback Error

    I have encountered error messages as below when I am running two d455 on my machine (realsense_ros 2.42.0): No stream match for point cloud chosen texture process - Color An error has occurred duri...

  • Frame drops in ROS using multiple d455 cameras

    Hello there, I'm running four d455 cameras in ROS in my project. All camera parameters are set to 1280*720 at 30 fps. But the result shows that all three cameras are fine while the last camera cann...