F Ricardo Auto
- Total activity 11
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 1
- Subscriptions 3
Posts
Recent activity by F Ricardo Auto-
Where does Dynamic Calibrator update the parameters
Hello. I am working with a D405. I installed the Dynamic Calibration Tool, and ran it once, everything goes perfect, but I notice that the calibration after the process was the same than before (re...
-
Depth maps
Hello. We are working with a D405 camera and having problems with depth measurement due to the poor surface texture. Looking at the RealSense software and using Python with deprojection method and ...
-
How can I create the depth_frame using RealSense SDK (Camera D405)
Hello I am having a holes problem in the depth_frame received from the SDK, because of the brightness in the surface. I use the two infrarred sensor to build the disparity map with openCV but the r...