Agan Simsek

  • Total activity 5
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Agan Simsek
  • Agan Simsek commented,

    There is a news like this. When the D435i is plugged into the USB port, a lag occurs in the entire system. For example usb joystick response times increase. By the way, I have not run an intel real...

  • Agan Simsek commented,

    I add to uvcvideo to blacklist. And It is OK now. Without any rebuild.

  • Agan Simsek commented,

    Hi MartyG, Thanks for the quick response and the eleccelerator wiki reference with nice explanations. I am aware of the support and experience you have shown here for a long time and on the intel r...

  • Agan Simsek created a post,

    realsenseROS with raspi

    Hello, I have problem Houston. I have a test setup with RasPi 4B and Ubuntu Server kernel 5.4. When I connect to USB3.1 port. I am getting below message with dmesg command. [ 6582.609156] usb 2-2: ...