Jdzitsiuk

  • Total activity 3
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Jdzitsiuk
  • Jdzitsiuk commented,

    Thanks Marty, this is the wavelength, right? I wonder about the frequency: for example I see that for D455 there are two options 57 KHZ and 91 KHZ in the API via RS2_OPTION_EMITTER_FREQUENCY. And w...

  • Jdzitsiuk created a post,

    IR projector frequency for D435i

    Hi, What is the modulation frequency of the IR projector in the D435i camera? I'm investigating IR interference issues with non-RealSense devices. Thanks,Jenna