Lschreurs25

  • Total activity 16
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 3

Activity overview

Latest activity by Lschreurs25
  • Lschreurs25 commented,

    Okay, I will try this.  For now I built a buffer for the height, which returns an average of the last 100 correct measurements. It isn't the correct way to fix the issue, but it must do for now. I ...

  • Lschreurs25 commented,

    Hey MartyG,   So I got the Jetson working again, only the problem remains. On top of that, the PC is having a similar problem. Where the Jetson gets incorrect depth measurements with little to no t...

  • Lschreurs25 commented,

    Okay I will look into this!   It seems there are some problems with the Xavier at the moment, which need to be fixed before I can test this. So when these are resolved I will get back at you!

  • Lschreurs25 commented,

    I have included CUDA support while building. So you are saying the line : "frames = frames.apply_filter(alignment); " is actually increasing the execution time as it is unnecessary? I will try thi...

  • Lschreurs25 commented,

    Hi Marty,   First of all, I think you tagged the wrong person, but yes my program uses wait_for_frames(), as seen in the screenshot along with the code used to get the frame.  

  • Lschreurs25 created a post,

    Incorrect depth measurement at high speeds

    So I have a computer vision program which uses the intel Realsense D435 camera for the depth measurements and for the RGB-image. The program is being developed on a PC with a strong CPU (i7-10700...

  • Lschreurs25 commented,

    Hi MartyG,   Thank you for your reply! I will try your answer and get back at you later this week. A little busy at the moment :).

  • Lschreurs25 created a post,

    Difference in initial seetings between devices?

    Hi all!   I have a question concerning the settings of a D435 camera. I have a computer vision program made with opencv(c++) and a D435 RealSense camera. I use a PC to do all the programming and de...

  • Lschreurs25 commented,

    So for anybody who comes across this post with the same problem: I found that the red pulsing happens with an exposure set between roughly 150 and 250. Any exposure above or below this does not cre...

  • Lschreurs25 commented,

    Yeah I meant 200 ms, not 20. There are fluorescent lights in here, but I tried putting the Power line frequency to 50, 60 and Auto, but all three options did not help the problem. I'll look into wh...