Smeekim

  • Total activity 3
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Smeekim
  • Smeekim commented,

    Hi MartyG. Here are the RGB image and depth map extracted from a bag file of intel d455.  The phantom was located at a distance of 3m from D455. But the depth measured by D455 was about 1.5m. 1.5m ...

  • Smeekim created a post,

    The unit of point clouds measured from D455

    Using D455 depth camera, we measured point clouds from a phantom placed at 3 m from the camera. But the depth measured by camera is almost 1.5 meters. Why the measured depth by D455 is different wi...