Lamlk1341

  • Total activity 11
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 3

Activity overview

Latest activity by Lamlk1341
  • Lamlk1341 commented,

    Are there max and min values for the subpixel in the above formula? Thanks

  • Lamlk1341 created a post,

    D455, purple tints under the sunlight

    I found that there were purple tints on the point cloud surveyed by D455 if under the sunlight. I also found that the other users got this problem too.  I want to know the reason about purple tints...

  • Lamlk1341 commented,

    Can I use those preset files in the Dot3D pro?

  • Lamlk1341 commented,

    Thank you so much! Regarding the depth resolution, the default setting is 848x480 for my D455, and with a warning message. Should I increase the depth resolution (to 1280x720) for acquiring a bette...

  • Lamlk1341 commented,

    Thanks for your prompt reply! I understand the theoretical limit for depth cameras now. Regarding D455, I found the baseline is 95mm and the HFOV is 87 degree according to the Page.55 in  "Intel Re...

  • Lamlk1341 commented,

    I have already installed the Dot3D on my Surface Go 2.  However, I cant find the cameras under the Device Manager nor Imaging Device. Thank you!

  • Lamlk1341 created a post,

    D455 connection problem

    I found that my Dot3D on Surface Go with original type-c cable frequently fail to recognized the D455. How to fix the problem? Thank you.

  • Lamlk1341 created a post,

    Z-accuracy for D455

    For D455, the Z-accuracy is smaller than 2%. (up to 4 meters) I was wondering what is the meaning of "smaller than 2%" for z-accuracy. Is that mean there are max. 2% differences between the measure...