1520870736
- Total activity 18
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Comments
Recent activity by 1520870736-
Yeah, I do not have confidence in the cable. But I have used the oscilloscope to watch the waveform of Pin-5 and Pin-9 and they looked like a sine wave while they were exactly the same. Is it possi...
-
Thank you!!! Really Appreciate your hep. I will contact with my supervisor instantly about this solution. Besides, there is not other way to sync the two cameras using the hardware? The situation n...
-
There is a project using two cameras at the same time. And I need to get the pictures from camera simultaneously. Currently, two cameras can not provide me with the pictures at the same time. Thus,...
-
-
I install the RealSense SDK using the instructions from a website called CSDN because the git clone method is not quite working well at that moment. And the which pin is what doesn't matter, becaus...
-
ROS Warning: Non-sequential Video and Metadata v4l buffers ideo frame dropped, video and metadata buffers inconsistency UVC metadata payloads not available. Please refer to the installation chapter...
-
And also, is it possible the voltage of sync(pin 9) and gnd(pin 5) are the same ? I can't detect any difference between two pins. They are both the same waveform in oscilloscope.
-
Still didn't work. Is it possible the connection is to be blame?qwq
-
And my changes on realsense-viewer are also shown below:
-
Obviously, their frame timestamps are not the same. So is this because the connection is not done yet?The connections are shown below: