Kakitsubata0711
- Total activity 8
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by Kakitsubata0711-
Kakitsubata0711 commented,
Hello Halim, Recently I found that we can download and install librealsense using Homebrew. (Command : brew install librealsense) Now librealsense 2.49.0 is installed. And I found that the big de...
-
Kakitsubata0711 commented,
Hello Halim, I would like to know how the stable resolutions and frame rates of RGB image and Depth image are when using L515 on MacOS. Could you please tell me the dictum? Best Regards, Masash...
-
Kakitsubata0711 commented,
Hello Halim, Thank you for your comment. Now I do not need the IMU data, so it is OK to stop the IMU data from the camera. Incidentally, is it possible to stop or kill the data output of IMU? I e...
-
Kakitsubata0711 commented,
Hello Sahira, Thank you for your comment. I have tried the packaged cable with the camera. MacBook has only Type-C ports, so I used the Type-C to A cable with a conversion connector. Incidentally...
-
Kakitsubata0711 created a post,
L515 Frame Rate with Macbook
Hello, I'm using L515 in Windows PC and MacBook. When I set the maximum sensor resolution, the big delay occurs and RGB image and depth image do not synchronize in MacBook. But in Windows PC, the...
-
Kakitsubata0711 created a post,
Error occurs when using L515 on Macbook
Hello, Now I'm trying to use RealSense L515 on Macbook. But it does not work well enough, so please give me advices. At first, my environment is as follows. MacBook Pro (13-inch, 2020, Four Thund...