Morphysmate

  • Total activity 7
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Morphysmate
  • Morphysmate commented,

    I get the same error using rs-fw-update. The fw update will only work with a version higher than 1.5.8.1, which does not and will never exist. This is a known problem with the realsense cameras. Th...

  • Morphysmate commented,

    This is the error I get when enabling the depth stream on v2.35.2. If I try to upgrade the firmware, I get the same error as before. The camera is locked and can only be upgraded to a fw version h...

  • Morphysmate commented,

    The problem persists. The issue is I cannot upgrade the firmware because the camera is locked from the 20 downgrade limit, so I am stuck on fw version 01.04.00.00. The firmware cannot be upgraded b...

  • Morphysmate commented,

    v2.48 installed on Ubuntu 18.04 LTS on a Jetson Nano. The camera isn't recognized with any higher version. I have it installed on a Windows 10 machine as well but realsense-viewer takes around 5 mi...

  • Morphysmate commented,

    After doing some more research, I've found bin to Intel Hex converters.  Theoretically would it be possible to disassemble that and interpret into C language with radare2 or something?  The goal wo...

  • Morphysmate created a post,

    L515 Locked Update Firmware Fails

    My L515 depth stream throws various errors or I get "no frames received" depending on what version of sdk used, while the latest doesn't recognize it at all.  The current firmware version is 01.04....