Tomek
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Tomek-
Tomek commented,
Base on the above photo, one can conclude that it is possible to detect small objects as washers. Do I understand correctly that the result of the photo made by the camera is exactly what you provi...
-
Tomek commented,
From your tests, one can conduct that there is no possibility to detect such small objects using RealSens cameras. There is one more thing which can be tested. If you could please put the camera in...
-
Tomek commented,
Thank you for detail explanation. Unfortunately, In my case, I can't use "classic" detecting methods on an image because I can't control the color of my "flat surface". For example, the surface can...
-
Tomek commented,
Hi MartyG. As far as I understand correctly: one the first photo you are using depth mode, on the second textured point cloud. I see the washers, but I don't know how can you recognize the theme. I...
-
Tomek created a post,
Can Intel RealSense depth camera recognize a small object (e. g. bolt washer) from distance 1m?
I have a use case in which I need to count small objects (e. g. bolt washer) which lie on a flat surface. The objects have a height of about 2 mm. The camera can be mounted parallel to the flat sur...