Katharina
- Total activity 8
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Comments
Recent activity by Katharina-
Hi Zulkifli, When I launch the RealSense Viewer, the preset does not automatically set to default. It automatically sets to "Max Range" and when I look at all the options in the drop-down menu, "De...
-
Do you synchronize the frames based on the best match of the timestamp (as you described) when I request "aligned" data? That is either color aligned with depth or depth aligned with color? Can I a...
-
I can't see "Default" as an option anymore when I launch the Intel Realsense Viewer. The only options I have are: Custom No Ambient Light Low Ambient Light Max Range Short Range Is "Default" simi...
-
Thanks for the answer! The link to the rs_options.h file is really helpful. I also managed to build the intel realsense viewer for OSx and was able to test some of the configurations. Are those con...