Eremteknoloji
- Total activity 12
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 4
Posts
Recent activity by Eremteknoloji-
about ros camera calibration and d435 on chip calibration values
hi Marty, how can I match the prx pry fx fy values in the output of the rs-enumerate-devices -c command with the fx,fy,cx,cy, d0,d1,d2,d3,d4... values in the ros yaml file.Thanks.
-
D435 Asic Temperature value is not valid!
I am getting this error while working with rs_camera.launch file. I am using sdk 2.47 and realsense ros 3.0 on odroid xu4 ubuntu 16.04. realsense-viewer ASIC TEMP=41. How can you help? Thanks.
-
Is slam application possible on raspberry pi 4 with t265 camera?
I want to use t265 camera with raspberry pi 4 for indoor drone application. Can I get enough slam performance from pi 4 with the camera t265? Or what are the alternative boards you would recommend.
-
Is slam application possible on raspberry pi 4 with t265 camera?
I want to use t265 camera with raspberry pi 4 for indoor drone application. Can I get enough slam performance from pi 4 with the camera t265? Or what are the alternative boards you would recommend.