Michael Schwaiger

  • Total activity 8
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 4

Activity overview

Latest activity by Michael Schwaiger
  • Michael Schwaiger created a post,

    ROI for authentication

    Is it possible or foreseen in later releases to define a region of interest that will only be used for finding faces and performing the authentication? It would be important to have such a feature ...

  • Michael Schwaiger created a post,

    Live preview image in full resolution

    Currently it seems that the SDK v0.15.0 only returns the live stream preview images in VGA (or similar) resolution. Will there be the option to return the FHD resolution without any additional rect...

  • Michael Schwaiger created a post,

    Match result details

    The Authentication result of the F455 currently only returns a boolean success value. Will it be added - and when - to the SDK that also the match score is returned via the API? At least I see a ma...

  • Michael Schwaiger commented,

    Do you have a timeline when this feature will be added to the SDK? It would be important to know for a decision if to go with F455 or not. Thx. Michael