Yu-Chern Peh
- Total activity 217
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 86
Comments
Recent activity by Yu-Chern Peh-
Hi E5119121b0, Yes, it is available in the link previously but now it has been removed. However, source code is still available which allows you to build. You can refer to the tutorial below:https...
-
Hi E5119121b0, Yes, it is available in the link previously but now it has been removed. However, source code is still available which allows you to build. You can refer to the tutorial below: ...
-
Hi Rukshan Fonseka, Intel® RealSense™ ID SDK is only validated on Ubuntu 18 with gcc 7.5+. Regards,Yu Chern
-
Hi Rukshan Fonseka, I am using Ubuntu 18.04 with default Python3 version, 3.6.9 and gcc 7.5.0. Regards, Yu Chern
-
Hi Alberto18 90, For your information, Intel RealSense T265 Camera has been discontinued. You can refer here for more information. The suggested alternatives for T265 are D455 and D435i. These ...
-
Hi Alberto18 90, The T265 camera's components such as the fisheye camera lens must be covered to minimize dust, humidity and personal contact such as fingers to lens. This is especially important f...
-
Hi Rukshan Fonseka, I also faced the same error when building Python wrapper with the latest RealSenseID SDK. However, using RealSenseID SDK version v0.23.0 worked for me. Sharing my steps: sud...
-
Hi Yxliuwm, Intel's own open-source RealSense ethernet networking project can be adapted for wi-fi according to its documentation. The project uses Raspberry Pi boards by default but the documentat...
-
Hi Xingxing, The development team are always working on further improvements and enhancements for future releases. However, we are unable to comment on any timeline, as it’s subject to changes. ...
-
Hi M Poderico, Just in case, the IMU specifications in T265 datasheet (page 12) might help. Regards,Yu Chern