Manuel Korell

  • Total activity 7
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 2
  • Subscriptions 2

Activity overview

Latest activity by Manuel Korell
  • Manuel Korell commented,

    Thanks for the quick response. Ubuntu machine and the Windows PC have the latest drivers. PC manufacturer PC model numberThe PC is custom built, but there is the specs:System: Host: manuel Kernel:...

  • Manuel Korell created a post,

    RealSense L515 Seems to be totally dead

    L515 is not recognized in either Windows 10 or Ubuntu 18.04. Compiled a fresh librealsense, the output with rs-fw-update -l is "there are no connected devices". My D435i works on the same cable if ...

  • Manuel Korell commented,

    Hi All. I have the same problem, L515 is not recognized in either Windows 10 or Ubuntu 18.04. Output with rs-fw-update -l is "there are no connected devices"My D435i works on the same cable if I ch...