Bbiehler
- Total activity 5
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Bbiehler-
Bbiehler commented,
Still no success. I started with the medium density presets, adjusted the exposure time and turned the laser power to its maximum, but did not see improvements: The red arrow points to the left wa...
-
Bbiehler commented,
So I changed the setup a bit: Distance to the objekt is now 0.1 m, resolution 848x480, and I worked with the disparity shift in the range of 40 to 150. The Depth units are 0.0001.Still the Post-Pr...
-
Bbiehler commented,
Yes, I can confirm that it is this U-shaped object. For a better understanding there is another picture of the extruded profile as seen from diagonally above and the part zoomed in from the other p...
-
Bbiehler created a post,
D435 won't detect small walls
I'm trying to detect aluminum profiles seen from the front side, as seen in the image below. I used the Threshold Filter to get rid of the background, played with the exposure and auto exposure an...