Zulkifli Halim
- Total activity 263
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 105
Comments
Recent activity by Zulkifli Halim-
Hi Liangkai, Thank you for reaching out to us. Are you able to view the depth image? Or both RGB and depth cannot be viewed? Sincerely, Zulkifli
-
Hello Yxliuwm, Thank you for contacting us. 1. For queue.enqueue(), is the thread blocked or just overwrite the oldest frame when the queue is full? queue.enqueue() adds an object to the end of...
-
Hello Michael, Sorry for the late reply. As of now, we don't have a Python wrapper for accessing the Translation parameter in Python. The Python wrappers are available here. Please refer to T2...
-
Hello Buck,Thank you for contacting us. The operating condition for the RealSense L515 camera is stated in Datasheet (section 4.5, page 17) In regard to how the L515 model measures depth, Intel ha...
-
Hello Dmeissner, Thank you for contacting us. We are discussing this issue via a private ticket. Sincerely,Zulkifli Halim
-
Hello Takashi, Please informed your customer that based on your description of the issue, your L515 is faulty and should be returned or exchanged. If you purchased the unit from the Intel Rea...
-
Hello Info,My apologies for the delayed response and thank you for sharing the video with us. Does something like this happen again when the camera is back to its initial position (before the came...
-
Hello Rachel,Thank you for contacting us. This might be due to the short range preset. This preset lower the laser power and gain so that close objects do not oversaturate the receiver. This allows...
-
Hello Lawrencehpy, Thank you for contacting us. The only available information for L515 dimensions is in the L515 Datasheet (Mechanical Specifications, page 19). We also provide CAD files for ...
-
Hello Walkerbalan1, Thank you for contacting us. We only have one lidar camera which is L515, it can be used to detect moving objects and large objects up to 9 meters away from the camera. It can...