Zulkifli Halim
- Total activity 263
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 105
Comments
Recent activity by Zulkifli Halim-
Hello Maurice,Thank you for contacting us.You need to place the license file at the same location as the Intel Realsense DIM Weight Software.exe file located. Sincerely,Zul Intel Customer Support
-
Helloo Christian Hubert, Greetings to you. You can test it but it probably will not work because Open Image Denoise only denoises images created with ray tracing, which RealSense does not do. T...
-
Hello Swider21,Thank you for contacting us.Yes, it is possible to activate the L515 camera on an Android device and the L515 only works via USB3.Regards,Zulkifli HalimIntel Customer Support
-
Hello Katharina, The latest version of librealsense The L500 Default preset has been deprecated. l500-options.cpp line 522 ""RS2_L500_VISUAL_PRESET_DEFAULT was deprecated!" );" Sincerely, Zulki...
-
Hello Guopengzhen2015, The description of the dws_create API in Section 2.1 Available Configurations of the file Intel_RealSense_DWS_v1.1.pdf, which is distributed with the DWS SDK, states that t...
-
Hello Katharina, The above assumes that there are no frame drops. Regards, Zulkifli
-
Hello Katharina, When you launch the RealSense Viewer, the preset will automatically set to default (see attachment). I suggest you look at the use full tips In L515 User Guide on page 18. Reg...
-
Hello Katharina, Thank you for contacting us. The synchronization between two streams from the same sensor like depth and IR should be perfectly synchronized by frame number. Synchronization ...
-
Hello Katharina, The configuration will back to default. The preset is set as "Default" when you launch the Realsense Viewer. Regards, Zulkifli Halim Intel Customer Support
-
Hello Katharina,Thank you for contacting us.The tools you mentioned are all included in the Librealsense SDK and the Linux Distribution can be installed here. Included in the SDK is a file that exp...