Yixun Liu

  • Total activity 154
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 53

Posts

Recent activity by Yixun Liu Recent activity Votes
  • rs2::frame_queue

    Hi, I have a couple questions regarding rs2::frame_queue. 1. For queue.enqueue(), is the thread blocked or just overwrite the oldest frame when the queue is full? 2. For queue.poll_for_frame(), it ...

  • Enable infrared stream

    Hi, In my application I need both depth stream and the left infrared stream. In my opinion, since the depth stream is generated based on both the left and  right infrared streams, so once I enable ...

  • An example CMakelists to config

    Hi, I built librealsense2.0 on Windows 10 using CMake and VS2017. To use librealsense2.0 in my project, I need to write the CMakelists.txt.  Can anyone give me an example? Thanks. Yixun

  • Point cloud flicker as rendering On Android

    Hi, As I render a point cloud I encounter the flickering sometimes. I have two threads. The main thread process the frames to generate the point cloud and then feed it to the OpenGL thread. The Ope...

  • is rs2::frame a unique smart pointer like unique_ptr?

    Hi,  From the following link: https://dev.intelrealsense.com/docs/frame-management "rs2::frame is a smart reference to the underlying frame - as long as you hold ownership of the rs2::frame the und...

  • Cannot find the API for pause and resume of Playback on Android

    Hi, I recorded a video into a.bag and want to use Playback device to play, pause and resume the video on Android. However, as I cast the parent class from Device to Playback I cannot find the pause...

  • Record streams of D435i on Android

    Hi, I use the following code to record streams. However, if I  config.enableRecordToFile("streams.bag"); the code will stuck at mPipeline.start(config). Without it the app runs smoothly. Is it beca...

  • Get pose stream from D435i

    Hi, I would like to get pose stream with D435i. As I know T265 can do this, but I do not want to use multiple cameras in my project. D435i can output IMU stream. I think I can output the Gyro and A...

  • FOV for different resolution

    Hi, According to OpenCV documentation:  https://docs.opencv.org/2.4/modules/calib3d/doc/camera_calibration_and_3d_reconstruction.html "If, for example, a camera has been calibrated on images of 320...

  • Replace the infrared or color sensor in D435i

    Hi, The color sensor in the D435i has small FOV. I am wondering can I replace it with a color sensor with big FOV? The depth FPS looks too slow if I use a big resolution than 640x480. Can you point...