Javier
- Total activity 42
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 4
- Subscriptions 14
Comments
Recent activity by Javier-
Thanks for the recommendation MartyG. Would you recommend using Clear Silicone Waterproof Sealant? (e.g. Loctite 908570)
-
Thanks for the clarification MartyX Grover So if the infrared projector improves the accuracy of the stereo matching algorithm, can we add an external IR projector to improve depth capturing even m...
-
I received an ETA update, they said it should be shipped by the end of November.
-
Really disappointing, its been 3 weeks, and the orders/support team have no idea when it will be restocked. Intel should stop receiving orders or mention that the product is in backorder.
-
Thank you Marty. It looks like is in backorder. This is what they replied: "We apologize for any inconvenience caused as the product you have ordered is in backorder. Rest assured we will ship the ...
-
MartyX Grover Is the Laser Power of the 400 Series in-built projector related to the Infrared? can we assume that this information is used to enhance the stereo matching algorithm?
-
Marty, The visual inspection of tightness alone cannot ensure the IP65 rating. Although I purchased waterproof cables from reputable brands like Amphenol and Bulgin, it's crucial to note that all t...
-
Wan, thank you for sharing this information. Just to confirm, can the D457 USB port perform and operate like the D455? (Assuming we follow your instructions). Some of us need the IP65 grade enclosu...
-
What is the reason that the D457 camera cant be used as a USB "plug and play" camera like the D455? Can someone (that is actually using the camera) confirm if the USB port can be used for developme...
-
was planning to use the D457 model for a volumetric measurement use-case in the construction industry. Any cost-effective way to work with the GMSL FAKRA interface?