Roman Leuzinger

  • Total activity 28
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 7

Posts

Recent activity by Roman Leuzinger Recent activity Votes
  • Longterm-Availability D430 and D4

    I heard a rumor that certain RealSense products would no longer be available for an indefinite period of time. What can be said about long-term availability? We currently use the modules: D430 (95...

  • Resource temporarily unavailable, number : 11

    We are testing the realsense on our robot and we are using ROS. At certain points, we change the exposure of the stereo camera periodically. Whenever we do that, the following error message is spam...

  • IR Filter Cutout

    Hello there, We are exploring the use of RealSense cameras in our product. We are looking into buying D435 modules but need an IR-Filter to be mounted. The D435f has a cutout for the dot projector,...

  • D430 integration (function of optical elements)

    We want to install the Depth Module D430 and the Vision Processor D4 in a customised housing.Do the left / right imager and the IR projector always have to be isolated with a gasket? Even if a two-...

  • D435F operation in darkness

    Hi In discussion with Intel Sales it was mentioned that we need an external IR illumination to operate our robot at night. However I did some trials with the D435F at night and was surprised about ...

  • Module D430 without RGB sensor

    The tech specification of the D430 is not so clear regarding RGB sensor. Therefore my questions: Does the D430 have a seperate RGB sensor? Same as the D435F?   Background of request: We achieve bes...

  • D457: GMSL to USB or Ethernet

    Hi Our autonomous robot bases on a SMARC SOM and a customized electronics. This provides USB2.0, USB3.0, Ethernet interfaces. On the SOM we are running ROS 1 Noetic.The D457 looks very suitable for...