1078258549

  • Total activity 6
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by 1078258549
  • 1078258549 commented,

    Dear MartyG.Thank you very much for your help and advice, we solved the problem by restoring the factory settings of the calibration data as you suggested and now the SDK depth values are perfect! ...

  • 1078258549 commented,

    Thank you for your reply!It's so bad that we tried your suggestion to turn on the time filter settings and change the "Smooth Alpha" from the default value of "0.4" to "0.1", while changed the pres...

  • 1078258549 commented,

    Thank you for your reply!We will turn on the time filter settings as you suggested and change the "smoothing alpha" from its default of "0.4" to "0.1".However, it should be noted that although ther...

  • 1078258549 commented,

    Thank you for your reply!1. Our RealSense SDK version is v2.42.02. Our firmware version is 05.12.11.003. We set the "Enable emitter" option in the side panel to "Laser"The above three points can be...

  • 1078258549 created a post,

    Large error in D435 depth values

    Dear Technical Support Staff.Hello!We are having some problems with the D435 depth camera for depth testing, when we do a depth visualisation test on realsense-viewer with a white wall we find that...