RealSense Support

I can't open the Intel.RealSense.Viewer.

Comments

1 comment

  • MartyG

    Hello, could you tell me please whether the Viewer window displays correctly if you launch Intel.RealSense.Viewer in Windows without the camera being plugged in?

     

    if the Viewer window is still blank when launching with no camera plugged in, then please try installing the full RealSense SDK on your computer with the Intel.RealSense.SDK-WIN10 installer program if you have not done so already.

    Once the full SDK has been successfully installed, please plug the camera in and then launch the RealSense SDK's rs-capture example program using the instructions at the link below to see whether rs-capture can correctly display the camera streams.  

    https://github.com/IntelRealSense/librealsense/issues/8024#issuecomment-747630656

    0
    Comment actions Permalink

Please sign in to leave a comment.