RealSense Support

Custom RGB position calibration seems unresponsive

Comments

1 comment

  • MartyG

    Hi Lucan Martin

    Have you used the CustomRW tool that is part of the Dynamic Calibration system to write a calibration to the camera hardware with its -w command, please?  Details about doing so can be found on page 58 of the Dynamic Calibration user guide.

     

    https://www.intel.com/content/www/us/en/support/articles/000026723/emerging-technologies/intel-realsense-technology.html

     

    That section of the guide also describes how a calibration can be exported to an xml format file, and the XML file also loaded back in so that the calibration in it can be written to the camera hardware.  So conceivably you could create an XML calibration file, manually edit it's contents in a text editor program and then load it back into CustomRW with its -r command and write the amended calibration to the camera with the -w command.

    0
    Comment actions Permalink

Please sign in to leave a comment.