View my account

D455 Install by rotating 90 degrees

Comments

5 comments

  • MartyG

    Hi Thakd037  You can physically orient the camera side-on.  However, if the image was rotated 90 degrees in the opposite direction using scripting then all calibration data and other parameters would need to be updated.  If you do not wish to perform such an adjustment of the image to re-orient it the 'right way up' though then it should be fine to place the camera at that angle.

    0
    Comment actions Permalink
  • Michael E Wescott

    I have two D455 cameras rotated 90 degrees.  I need to detect april tags and human presence in a zone offset from the april tag.  I believe I will need to rotate the images but I need to know what the best way is to do this and still have the 3D detection capability.  I read a post that mentioned that there was a proposed SDK change to handle it from two years ago.  Was that ever implemented?

    0
    Comment actions Permalink
  • MartyG

    Hi Michael E Wescott  A new mechanism for rotating the camera frames using a post-processing filter was merged into the development branch of the librealsense SDK three days ago at the time of writing this.

    https://github.com/IntelRealSense/librealsense/pull/13499

    https://github.com/IntelRealSense/librealsense/tree/development

    0
    Comment actions Permalink
  • Michael E Wescott

    Thanks. Do you know if that is compatible with the ROS 2 wrapper? Can it run on a NVIDIA Jetson ORIN NX with Jetpack 6.0?

    0
    Comment actions Permalink
  • MartyG

    There is not further information currently available about this librealsense SDK post-processing filter.  You could post a comment at the discussion at the link below to register your interest in ROS2 support for the filter.

    https://github.com/IntelRealSense/librealsense/issues/6023

    0
    Comment actions Permalink

Please sign in to leave a comment.