Oscillations in the distribution of depth
Hi,
we noticed an unexpected problem while trying to track a fish in a bowl. When looking at the distribution of depth values, we can observe oscillations where some values are more often found than others.

This is unexpected because our fish is supposed to explore the whole space and not some discreet positions in the vertical direction.
To confirm that the problem was coming from the camera, we designed a simple protocol. We attached a small red LED on a CNC rail, that is moving away from the camera. The LED is moving 1mm per step and at each step we are acquiring 10000 images.

This simple protocol gives rise to similar oscillations. We are a bit lost here. We haven't seen anybody reporting similar issues. Would there be a simple explanation why the depth distribution is not homogeneous?
thanks
-
Hi Renaud Bastien The camera can have difficulty reading depth detail from reflective surfaces such as the glass of fish aquariums. If the camera is outside of the bowl then aligning depth to color can help to improve results.
If the camera is immersed in water then the camera may need to be calibrated for that environment in order to account for distortion caused by the water. There is an extensive technical discussion about this subject at the link below.
https://github.com/IntelRealSense/realsense-ros/issues/1723
The project FishSense is an example of fish monitoring and measuring with an immersed RealSense camera.
https://www.youtube.com/watch?v=KA_x03_Aru8
Which RealSense camera model are you using, please?
-
There was a recent case at the link below where an LED was being measured at 60 cm distance from the camera and they were experiencing "depth jitter" variation in the measurements. Their depth image showed that the bright LED light showed up but the rest of the scene's depth detail was mostly missing.
https://github.com/IntelRealSense/librealsense/issues/10429#issuecomment-1107853739
They confirmed that depth measurement jitter was significantly reduced if the camera's IR dot pattern projection was enabled. Is the projector on your own camera enabled or disabled, please?
Please sign in to leave a comment.
Comments
3 comments