RealSense Support

Change D435i frame size/resolution with Unity asset

Comments

4 comments

  • MartyX Grover

    Hi Puechjg  May I confirm please if you are changing the resolution before you click the 'play' triangle to run the program, since it is not possible to change the resolution after the program has started running.

     

    If you are able to change the settings, could you try setting the FPS to '6' when using 1280x720 resolution.  This will help to confirm whether or not the camera is being mis-detected as being on a USB 2 connection instead of USB 3 in Unity, since the supported resolution / FPS modes will be more limited when the camera is in USB 2 mode.

    0
    Comment actions Permalink
  • Puechjg

    Thank you very much for your clear and instant answer. It works with 1280x720@6fps so it fits the requirements of my application.
    Is there a documentation with all allowed resolution/fps profiles for differents USB standards ? Our clients can have any setup so it will help us to reach the best performance.

    I thank you again for your help !

    0
    Comment actions Permalink
  • MartyX Grover

    You are very welcome!

    Pages 70-77 of the current edition of the data sheet document for the 400 Series cameras list all supported resolution and FPS combinations on USB 2 and USB 3 for particular 400 Series models

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet

    0
    Comment actions Permalink
  • Sujeet Jha

    Hi, i'm also facing the same issue only 640x480 is working for me my device is d455f can you please help?

    0
    Comment actions Permalink

Please sign in to leave a comment.