View my account

[D455] How to extract each image photographing by Right Imager and Left Imager

Comments

5 comments

  • MartyX Grover

    Hi Hgkim  Yes, you can extract infrared images from both the left and right imager with the RealSense Viewer program or with your own script.  You can obtain frames individually or record a moving stream of them into a bag file like a video recording of camera data that is treated as though it is a live camera when played back.

    0
    Comment actions Permalink
  • Hgkim

    Thanks for the reply.

    I want to 2 images about same frame.

    2 images are RGB color image which is exported by left imager and right imager. 

    I will use them to compare the accuracy with commercial products through my depth estimation calculation.

    So we need RGB images extracted from the left and right imagers of the same frame.

    I extracted the bag file and looked at it, but I couldn't get the function I wanted.

    Can I get RGB color images extracted from each left and right imager?

     

    Best regard,

    Honggi KIM

    0
    Comment actions Permalink
  • MartyX Grover

    RealSense 400 Series cameras only support RGB color from the left imager and only on the D405, D415 and D455 models.

    0
    Comment actions Permalink
  • Hgkim

    Thanks for your comments, MartyG.

    To make sure, do you mean we can only get the color image captured from the left imager?

     

     

    0
    Comment actions Permalink
  • MartyX Grover

    Yes, I can confirm that a color image from the infrared sensor instead of the RGB sensor can only be provided by the left infrared sensor on camera models that support it.

    0
    Comment actions Permalink

Please sign in to leave a comment.