RealSense Support

Complete 3D Scene Scanning with D455

Comments

1 comment

  • MartyX Grover

    Hi Jkchen2. Thanks very much for your questions.

     

    1 and 2.  The open-source RealSense SDK example program rs-kinfu (KinectFusion) that is based on C++ and OpenCV may meet your needs.  A single camera can be moved around a scene, progressively building up a pointcloud scan of the scene by fusing frames.  Once you are satisfied with the amount of detail on the scan, you can export it as a .ply format pointcloud file that can then be imported into 3D modelling software for conversion to a solid model.

    https://github.com/IntelRealSense/librealsense/tree/master/wrappers/opencv/kinfu

     

    An example of an open-source 3D software that can be used with RealSense .ply files is MeshLab.

    https://www.meshlab.net/

    https://www.andreasjakl.com/capturing-3d-point-cloud-intel-realsense-converting-mesh-meshlab/

     

    3.  In my experience, the number of people who create their own approach of recording a ply and then converting it to a solid mesh with open-source solutions is greater than the number who use commercial software to do so.  Neither approach is incorrect though and simply depends on your preferences and project requirements / budget.

    Tracking the camera position is usually not required for scene scanning applications.

     

    4.  A type of large scale scene modelling that can benefit from an IMU (gyro and accelerometer) is SLAM.  A moving camera, typically attached  to a mobile robot can navigate a patrol route through rooms, recording a point cloud map as it travels.  When you are satisfied with the amount of detail on the scan, the recording can be stopped and saved.

    Intel provide a SLAM map recording tutorial for ROS that utilizes the IMU.  It was designed for the D435i camera model but should work with D455 too.

    https://github.com/IntelRealSense/realsense-ros/wiki/SLAM-with-D435i

    Whilst it does not feature relocalization, a RealSense user created their own version of the guide that adds relocalization and relative camera position tracking and plotting.

    https://wshinkansan.github.io/2019-UGRP-DPoom/SLAM.html

     

    Other open source SLAM solutions are compatible with RealSense cameras.  A couple of examples are ORB-SLAM (such as ORB-SLAM2 and ORB-SLAM3) and Kimera.

    0
    Comment actions Permalink

Please sign in to leave a comment.