RealSense Support

Inconsistency with D415

Comments

1 comment

  • MartyX Grover

    Hi Dpalumbo573. The strip of invalid data at the left edge of the image is normal and is called the Invalid Depth Band.  Page 79 of the current edition of the data sheet document for the 400 Series cameras provides information about it.

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet

     

    In regard to depth fluctuations, the depth reading can be made more stable by using a Temporal Filter post-processing filter and setting its Smooth Alpha to a low value such as '0.1' instead of its default value of '0.5'.

     

    There may be factors in the environment of the location that the camera is being used in that may be contributing to the fluctuations though.  Could you provide an RGB image of the scene to help to identify elements in the scene that are potentially disruptive, please?

    0
    Comment actions Permalink

Please sign in to leave a comment.