RealSense Support

D435 Frame Delay

Comments

5 comments

  • MartyX Grover

    Hi Adrian, may I first confirm whether your 8 cameras are attached to two industrial USB 3.2 hubs of the same model (the USB standard allows up to 5 hubs to be linked together).

    If 4 of the cameras are not attached to another hub of the same model then the two sets of 4 cameras would likely be using two different brands of USB controller, introducing potential unpredictability into the USB system in regard to how one set of 4 cameras will behave compared to the other set.

    0
    Comment actions Permalink
  • Adrian

    Hello Marty, I can confirm that all 8 cameras are attached to two identical industrial USB 3.2 hubs. 4 cameras per hub, and each hub is connected directly to the host computer. I've also used the same cables and power supplies for the hubs.

    0
    Comment actions Permalink
  • MartyX Grover

    Although it is recommended practice to use poll_for_frames() with applications that access multiple cameras, it also has the drawback that you need to control when the CPU is put to sleep and for how long, otherwise the CPU can max-out its utilization percentage at 100% of a single core, which could account for the delay effects that you are encountering.  This is described by a RealSense team member at the link below.

    https://github.com/IntelRealSense/librealsense/issues/2422#issuecomment-423254709

     

    Although poll_for_frames() is the recommended instruction for multicam applications, some RealSense users who have created multiple camera applications whose processing is not too demanding have opted to use wait_for_frames() instead and found that it did not have a negative effect on performance.  Control of CPU sleep periods is not required with wait_for_frames()

    0
    Comment actions Permalink
  • Adrian

    Hi Marty,

    Thank you for your prompt responses and suggestions. I tried a little experiment with wait_for_frames today and it did not seem to make a significant change. I also reviewed my use of poll_for_frames() and I have little concern about CPU usage.

    In my testing today I was able to reproduce my issue. It seems like poll_for_frames() is simply returning False for an extended period of time. The issue resolved after I disconnected and reconnected all of my cameras.

    This leads me to a couple of additional questions for you:

    Is there a way to query the state of the camera's FW? Perhaps some logs, or at lease some indication of whether the camera might be in some state where it is unable to provide frames?

    Do you think there could potentially be an issue with connecting 4 d435 cameras to a single hub? From what I've read in the whitepapers and given the resolution and frame rates I'm using, this didn't initially seem to be an issue. However, given the fact that I was able to resolve simply by reestablishing the USB connection would seem to indicate that the USB topology could be the source of the problem.

     

    Thanks

    0
    Comment actions Permalink
  • MartyG

    Using 4 cameras per hub at 6 FPS should not be exceeding the average 5 Mbps maximum bandwidth of a typical USB hub.

     

    There have been rare past cases where the stream has timed out or experienced other errors when 6 FPS is used because frames were not arriving quickly enough.  In such cases, increasing the FPS to 15 made the problem disappear.  

     

    If exception type errors are generated by the timeout then you could implement an error try-catch to initiate a pre-programmed action if an exception error occurs, such as triggering the hardware_reset() instruction to automatically reset the camera instead of having to unplug-replug it.

    https://dev.intelrealsense.com/docs/librealsense-error-handling-scheme

    0
    Comment actions Permalink

Please sign in to leave a comment.