Lenovo Miix700 12isk built in Camera not working in Windows10 or Ubuntu 26.04
Hello,
I have old Lenovo ideapad Miix700 12isk laptop. Before I deleted window 10 and install Ubuntu 26.04 camera was working. I removed windows 10 and installed ubuntu 26.04. The built in camera now not working in Ubuntu or windows 10(I installed window 10 on different hard drive). I went through ubuntu help center all related Q&A but nothing seems to work. I can attached usb camera and that is working with cheese.
Thank you,
Harish
-
Hi Harish Shelat The Lenovo Ideapad Miix700 12isk was released in 2016 and so the RealSense depth camera camera that is built-in is the R200 model. Typically, manufacturers who build RealSense into their products pre-install the camera drivers into the computer so that it is ready to use when the computer is bought. This means though that if the computer is wiped to install another OS then the pre-installed camera drivers will be lost.
The current generation of RealSense SDK software does not support the R200 camera. In that era, R200 was intended to be used with Ubuntu 16.04 and did not have support created for later Ubuntu versions.
The best option for R200 users is to install the original librealsense1 SDK, though it was not designed for OS versions newer than Ubuntu 16.04 or Windows 8.1.
-
Hi Harish Shelat Do you require further assistance with this case, please? Thanks!
Please sign in to leave a comment.
Comments
2 comments