RealSense Support

Inquiry about RealSense D457 depth capture issue on glossy black automotive bumper

Comments

2 comments

  • MartyX Grover

    Hi joosung lee D457 has a minimum depth sensing distance of around 50 cm, so it is appropriate for use at 50 to 60 cm range, though a 

     

    It is a general physics principle (not specific to RealSense) that dark grey or black absorbs light and so makes it more difficult for depth cameras to read depth information from such surfaces.  The darker the color shade, the more light that is absorbed and so the less depth detail that the camera can obtain.

     

    Casting a strong light source onto such surfaces can help to bring out depth detail.  If the surface is glossy though then this could cause reflective glare that also makes it difficult for the surface to be analyzed by the camera for depth information.

     

    Spraying the bumper with an anti-reflective aerosol spray like the kind used when photographing jewellery for catalogs could help to dampen reflections.  The link below has an example of such a product.

    https://www.laserdesign.com/3d-scan-spray/?language=en_US

     

    I would first though recommend trying increasing the RealSense Viewer's Laser Power setting under Stereo Module > Controls to its maximum value of '360'.  This increases the visibility to the camera of the invisible IR dot pattern projection cast onto surfaces by the camera, which aids depth analysis.

     

    If changing the camera model is an option then as long as you do not need to fit the entire bumper into the viewpoint of the camera then the D415 model would be recommendable.  It excels at accurately scanning stationary objects and has 2x better depth accuracy / 2x less depth noise than other models in the RealSense 400 Series range.  It also supports 1280x720 depth and RGB resolutions by default.

    0
    Comment actions Permalink
  • MartyX Grover

    Hi joosung lee  Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.