Missing calibration target printable
Hi,
I was reading the following whitepaper on self-calibration:
, which states:
Included here are two versions of the ground-truth target, designed for printing onto standard 8 ½ x 11” or 11 x 17” paper.
However, I could not find those attachments on the page.. Could you point them to me, or add those into the page so they are downloadable? Thanks!
Best,
Weinan
-
Hi W Si
The RealSense SDK release notes for the 2.50.0 SDK version have a link to the focal-length and tare target in PDF format. This PDF is configured for 8.5x11" dimensions.
https://librealsense.intel.com/Releases/UCAL/Calibration_Target_v1.pdf
Please sign in to leave a comment.
Comments
2 comments