RealSense Support

Guidance on merging point clouds from two RealSense D455f cameras for telepresence

Comments

5 comments

  • MartyX Grover

    Hi Moamen Ali  Thanks very much for your questions.

     

    1.  There is more than one approach available for calibrating cameras together.  It could be done with program code, or with ROS.  

     

    2.  Hardware sync is not required for creating a combined pointcloud.

     

    3.  Multiple RealSense 400 Series cameras do not interfere with each other.

     

    4.  RealSense provide an official example in the C++ programming language at the link below for using two devices to "stitch" their viewpoints together in order to generate a combined pointcloud.  The method uses a tool called MATLAB to calibrate the cameras together.

    https://github.com/realsenseai/librealsense/blob/master/wrappers/pointcloud/pointcloud-stitching/doc/pointcloud-stitching-demo.md

     

    Alternatively, another RealSense example, that is in the Python language, is box_dimensioner_multicam, which can calibrate multiple cameras together by calculating the spatial relationship between them and creating a point cloud from the depth frames of all the cameras.  It does not actually visibly output that cloud though, so you may have to modify the program if your application requires a visible on-screen cloud.

    https://github.com/realsenseai/librealsense/tree/master/wrappers/python/examples/box_dimensioner_multicam

     

    Another RealSense example, in C++ language, is rs-kinfu.  Instead of using two fixed position cameras though, it uses a single camera to build up a pointcloud in real-time by moving the camera around.

    https://github.com/realsenseai/librealsense/tree/master/wrappers/opencv/kinfu

    0
    Comment actions Permalink
  • MartyX Grover

    5.  In regard to minimizing latency and optimizing stability, you should use a computer that can handle two RealSense cameras simultaneously.  Most PCs can cope with this, but low-end development boards (single-board computing devices) may struggle.  If you plan to use a development board, an Nvidia Jetson board such as Jetson Orin Nano is recommendable.

     

    Depth stability can be affected by a range of environmental factors.  Try to avoid pointing the camera at dark grey / black colored surfaces which may not be picked up by the camera and also avoid reflective surfaces.  Also do not use the camera in an office room with fluorescent ceiling strip lights if possible as it can result in noise on the depth image.

    0
    Comment actions Permalink
  • Moamen Ali

    Dear MartyX Grover,

    Thank you very much for your detailed response and for sharing the RealSense examples.

    I would like to clarify that my current implementation is being developed in Unity. I am using two Intel RealSense D455f cameras, and my goal is to generate a point cloud from each camera and merge both point clouds into a single unified 3D representation inside Unity in real time.

    Could you please advise whether the calibration matrix generated using the rs-pointcloud-stitching workflow can be used directly in Unity to transform the point cloud from the second camera into the coordinate system of the first camera?

    Also, if there is a recommended workflow for applying the extrinsic calibration result inside Unity, I would really appreciate your guidance. For example, how to correctly convert the rotation and translation values into a Unity Matrix4x4, and whether any coordinate system conversion is needed between RealSense and Unity.

    Any advice, sample code, or recommended approach for implementing this multi-camera point cloud merge specifically in Unity would be very helpful.

    Thank you again for your time and support.

    0
    Comment actions Permalink
  • 0
    Comment actions Permalink
  • MartyX Grover

    Hi Moamen Ali  Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.