View my account

Using Two RealSense Cameras Facing the Same Scene: Depth Interference Concerns?

Comments

1 comment

  • MartyX Grover

    Hi JINGJING LIU  Multiple RealSense 400 Series cameras do not interfere with each other and overlapping their fields of view can actually improve depth analysis.  This is because each camera projects a pattern of invisible IR dots that the camera uses to aid depth analysis of surfaces.  When the dot pattern projections from two cameras overlap it increases the density of the pattern in the area where the views overlap, which is beneficial to depth analysis.

     

    The RealSense models that could experience interference from multiple cameras were the SR300 and L515, which are retired and no longer available.

     

    Although 400 Series cameras do not interfere with each other, they can interfere with non-RealSense IR devices nearby, such as card reader devices and wireless mice, or non-RealSense cameras that use IR.

    0
    Comment actions Permalink

Please sign in to leave a comment.