RealSense Support

RF interference / limitation on Intel RealSense D435i

Comments

4 comments

  • MartyX Grover

    Hi Jet Easy  RealSense cameras do not experience RF interference and can be used in industrial and radioactive environments.

     

    If you choose to use your own choice of USB cable with the camera instead of the official 1 meter one provided with the camera then it should be a shielded cable in order to avoid interference with radio reception.

     

    If you have devices in the vicinity to the camera that operate based on wireless IR principles then although the RealSense camera does not experience interference from those non-RealSense devices, it may interfere with their IR in return.

    0
    Comment actions Permalink
  • Jet Easy

    Hi,
    Thank you for the explanation.
    So in simple terms:
    The RealSense camera itself is not affected by RF interference, even in harsh environments.
    However, the USB cable must be shielded, otherwise it can pick up interference.
    And while other IR devices do not disturb the RealSense camera, the camera may interfere with them.
    I have one additional question:
    Would you expect the same behavior when testing the camera inside a GTEM (ETS-Lindgren) cell with a frequency sweep from 300 MHz to 3100 MHz?
    This would help me better interpret my EMC test results.

    0
    Comment actions Permalink
  • MartyX Grover

    I am not familiar with ETS-Lindgren's GTEM test cells, though a review of their range of cells on their website gave me a basic understanding of what you are asking.

     

    There is not formal test data about exposure of RealSense cameras to environments with RF, EM, radioactive emissions and magnets.  The cameras have been used by our customers in all of those scenarios though with no reports of negative effects on the camera hardware or the images it produces during the now eight-year history of the RealSense 400 Series camera range. 

    0
    Comment actions Permalink
  • Jet Easy

    Thanks for the information. That gives me a better understanding of the situation

    0
    Comment actions Permalink

Please sign in to leave a comment.