RealSense Support

Comments

2 comments

  • MartyX Grover

    Hi Gil Gefen  If you would like to incorporate a D435's technology into your device then two circuit boards are required, the D430 Depth Module and the Vision Processor D4 V1 Board.

    These two boards are joined by an interposer connector.  This can be either a rigid circuit board or a flexible cable.  The cable approach will enable you to choose where inside your device's casing the boards are mounted, and the cables are available in a few different lengths (50mm, 100mm, 150 mm).  The 50 mm interposer cable is available from the official online RealSense Store.

     

    However, please note that combining these two boards will result in a D430 that has depth and infrared capability but not RGB color capability.  This is because in the D435 camera the RGB sensor is attached separately via a cable and these RGB sensor and cable components are not available for purchase separately for use with a D430.

     

    It is possible to add your own choice of RGB sensor if the sensor is a MIPI CSI-2 module so that it is compatible with the Vision Processor D4 Board.

     

    The D415 and D450 depth modules have the RGB sensor integrated on the depth module.  If the D415 is combined with the Vision Processor D4 V1, or the D450 is combined with a D4 V3, this will result in your device having the equivalent of a D415 or D455 camera, which do have RGB color capability.

    0
    Comment actions Permalink
  • MartyX Grover

    Do you require further assistance with this case, please?  Thanks!

    0
    Comment actions Permalink

Please sign in to leave a comment.