RealSense Support

RealSense D555 Camera Not Recognized After Firmware Update

Comments

1 comment

  • MartyX Grover

    Hello,

     

    If the cameras are not detected when only the USB cable is plugged in and the PoE ethernet cable is disconnected then the cameras may have become inoperable.  There is unfortunately no way for users to restore the camera with a rollback if it cannot be detected due to a firmware related failure.

     

    If they were bought less than 12 months ago then you should contact the retailer that it was purchased from to enquire about an RMA return for a replacement under warranty.

    0
    Comment actions Permalink

Please sign in to leave a comment.